Tool/software:
Hello,
I wonder if it is possible to generate a test tone from the DC209 board alone without the FPGA JESD board underneath? I just want to put out a simple tone onto one of the RF TX lines. I have attempted to do this after doing a GUI bringup using the console to write into SPI registers, and although I seem to be able to read and write successfully to the SPIA, I can't seem to be able to achieve the test tone output. I wonder if there is a different GUI available that would have the option to generate a tone within it or within the python script?
Thanks.