Part Number: AFE8030EVM
Other Parts Discussed in Thread: TSW14J58EVM
Tool/software:
The Latte software detects the board correctly on the startup screen, as well as the necessary drivers. However, once the script bringup.py is executed, the following errors appear in the terminal:
libpng warning: zTXt: Data error in compressed datastream
Deleting Handle..
Connecting...
ERROR: Please check environment setup! No device is detected.
FTDI Not Connected
FPGA not connected. Function reset skipped.
FPGA not connected. Function checkVersion skipped.
FPGA not connected. Function fpgaTxConfig skipped.
FPGA not connected. Function selectDrive skipped.
FPGA not connected. Function fpgaRxConfig skipped.
FPGA not connected. Function selectCapture skipped.
FPGA not connected. Function fpgaJesdReset skipped.
FPGA not connected. Function fpgaSysref skipped.
FPGA not connected. Function fpgaSysrefCheck skipped.
Also, the following errors appear in the Lattex log window.
Reset the FPGA and try again.
Couldn't find the proper FPGA settings. Try to change setupParams.fpgaRefClk to be a factor of lane rate.
Couldn't get the link up for device RX: 0
Couldn't get the link up for device RX: 1

I'm working also with the TSW14J58EVM board, DC128_A10
I look forward to your response, and I apologize for the inconvenience.