Part Number: AFE7950
Tool/software:
I would like to get some information regarding the Tx output power of the AFE7950.
Here is the graph in the datasheet:

There are 4 curves.
Is each curve related to one of the 4 channels while the other channels are set to OFF ?
For instance: the red curve is for 2TX
- Does it mean that only the channel 2 is transmitting while the other are OFF ?
- or does it mean that 2 channels are transmitting together while the 2 others are set to OFF ?
- or does it mean that the 4 channels are transmitting together and only the power is checked at the 2nd channel ?
I think it is related to one channel only, but I would like a confirmation for that.
Is there a graph where the 4 channels are transmitting together and we can see the output power at each channel ?