Dear team,
I am using the LMK04832-SP part and VCXO as Clk input.
I am using the DC coupled LVCMOS input as CLKIN,whether CLKinX* input should be directly connected to GND or through capacitor for DC Coupled input option.
Dear team,
I am using the LMK04832-SP part and VCXO as Clk input.
I am using the DC coupled LVCMOS input as CLKIN,whether CLKinX* input should be directly connected to GND or through capacitor for DC Coupled input option.
Hi Venkat,
Both the LVCMOS and Bipolar input options are internally AC-coupled, meaning that you can AC couple your unused input to GND (you could, in theory, DC couple it, but AC coupling it would reduce potential noise).
Consult Figure 9-5 that you have attached above.
Thanks,
Michael