This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7769EVM: Data accqusition from the AFE7769EVM

Part Number: AFE7769EVM
Other Parts Discussed in Thread: AFE7769

Dear TI Team,

I am planning to purchase the AFE7769EVM and would like to understand how to acquire IQ samples from the system. Is there any Python code, API, or software available for collecting and transmitting data?

Additionally, are all four Tx and four Rx channels synchronized by default, or any external clock required to achieve synchronization?

Is there a built-in GUI available for control and data capture? Also, could you please point me to the relevant datasheets or user guides?

Thank you.

  • Hi Purna,

    Thanks for your inquiry. Can I please learn more about your application and what you are planning to use the AFE7769 for? Please help share the following

    1. Frequency band(s)/range:
    2. IBW:
    3. Is DPD/CFR required:
    4. Project timeline:
    5. Volume:

    We have a script-based software used to configure the AFE7769EVM, with some of our other devices having a GUI-based software which is more intuitive. I would like to get insight into the above first though to ensure we provide you with the best evaluation module for your platform.

    BR,

    Simran

  • Hi Simran,

    Thank you for your Response

    Please follow the Details are given below

    1. Frequency band(s)/range:   400MHz  to 6GHz ( Wideband )
    2. IBW:   100MHz
    3. Is DPD/CFR required:  NO
    4. Project timeline:  Immediate
    5. Volume:   2


    Regards,

    Purna