Other Parts Discussed in Thread: TRF370417, DAC3484, DAC3482, DAC34H84
Hi,
Got a question from a customer about using and I/Q modulator like the TRF370417 in an AM modulation type of setup. I'm not an RF guru, so your inputs are welcome. Here is the statement from my client:
I might have an application requiring I/Q vector modulator for my next project starting from 110MHz and to 340MHz (this application uses AM modulation for Air Traffic Guidance equipment), I think that I can use I/Q vector mixer to control phase of side band of AM and its amplitude (side bands are at 90Hz and 150Hz modulates RF carrier in between 110MHz to 340MHz under Amplitude Modulation mode, or you can see it as AM carrier that has side bands at +/-90Hz and +/-150Hz offset from carrier); AM spectrum should as per plot below if you ignore intermodulation caused by a non-linearity of high power amplifier at 60Hz, 240Hz, 300Hz, and 180Hz; Design architect and approach is not designed yet and nothing has been started yet. I used I/Q vector modulator for QPSK type for direct conversion but not quite sure how well it works under AM.
Any feedback would be appreciated if this is a valuable option.
Thanks,
Alex