Hi,
Please give me the answers of following questions
1. The BB Tx Formatter mode can support three modes Byte, Nibble and Serial. According to the datasheet it is written that Max. clock interface rate/ channel
Byte Mode --> (clk x 4/4)/N; max 192.31 MSPS total (for all channels)
Nibble Mode-->(clk x 4/8)/N; max 125 (Nibble 0) and 96.15 (Nibble 1) MSPS total
Serial Mode--> (clk x 4/16)/N; max 48.07 MSPS total
How these rates are coming? Please give me the calculations regarding this. Also please tell me what is the significance of 4/4, 4/8 and 4/16?
2. When each DDUC is supporting 12 channels and 8 nibbles format the max IQ rate/ channel is 5.208e6 Mbps (assuming max baseband rate 500 Mbps). So due to PFIR if we consider 80% BW, so it is coming 4.16 MHz BW/ channel. So whether it means that each DDUC is supporting 4.16*12= 49.92 (>37) MHz of BW?
3. In High BW mode the max. BW supported by GC5337 is 37 MHz x 4=148 MHz, if we consider all the 4 DDUCs are behaving as DUCs. So in that case if any drawbacks are there?