Hello sir,
When we are using GC5330/37 for only ET purpose,
1) Is the sampled output of PA needed for GC5330/37 for ET operation only?
2) Since I have only low power upconverted RF as input, Is it possible to use IQ demodulator with ADC's output as baseband data input to GC5330/37 for ET operation only ?
3) To configure GC5330/37 for ET functionality what are the peripherals required ?
Regards,