Other Parts Discussed in Thread: TRF3765
I'm reading the documentation of the trf3765 and am struggling with an ambigous statement therein. On page 35 I read "Then, calculate the maximum frequency to be
input to the digital divider at fN. Use the lower of the possible prescaler divide settings, P = (4,8), as shown by Equation 6."
The sentence as written might imply that one should select the prescaler in such a way that fN,Max does not exceed 375 MHz. But this contradicts that the prescaler has already been selected by Equation 5. Furthermore, the PLL_DIV_SEL calculation will always lead to an fPM requiring the 8/9 prescaler, rendering the 4/5 prescaler useless.
Can somebody make some clarifying statements on this issue?