Other Parts Discussed in Thread: TRF372017, TRF372017EVM, DAC3283EVM
Hi there,
We are working on a project about a communication test set. We want to use the IQ modulator TRF372017 but here are some questions, hope someone can give us answers soon.
1. Can it injects a signal directly into the IQ pins?
2. The TRF372017 seems to have an oscillator built into it. Correct?
3. There is a reference clock input. Do we need to connect a reference oscillation signal directly for the TRF372017 to produce the quadrature RF signal? What value do we need for the reference clock? Where is it coming from, and what is it in reference to?
4. Is the board (TRF372017EVM) recommended for the quad-modulator populated and functional?
5. What kind of co-axial cable recommended for IQ connection (TRF372017EVM)?
Thank you.