hello,
We are using GC4016 in our project. Our requirement is GC4016 chips of two identical units shall get synchronised. To achieve this we have applied common clk to GC 4016. This chip is used in wideband mode. Independent units are working fine but they are not getting synchronised. pl help us in solving this.
We have configured sync controls of all blocks to SIA. SIA is derived using glue logic in FPGA. Both the chips are configured by processor with some time differance and chip generates SO signal. FPGA present in each unit will assert SIA when SO is generated. The SIA raising edge will occur with common sync pulse applied to two boards. We have monitored the raising edge of SIA in both the units and they are synchronised. We are testing this by applying common input signal to both the units using splitter. We have configured DDC chip as below
diag sync = always
OUPUT_SYNC = one_shot
counter_sync = SIA
os_mode =1
one_shot : it is made one by processor after configuring all registers, before releasing reset
CNT = 9 (TC is not used any way)
phase_sync = SIA
frequency_sync = SIA
nco_sync = SIA
dither_sync = SIA
zero_pad_sync = SIA
dec_sync = SIA
flush_sync = SIA
gain_sync = always
peak_sync = always
out_blk_sync = SIA
GC4016 i/p is real mode from ADC and output is synchronous serial o/p in complex mode.
dec value is 5 and decimation ratio is 9.