Hello,
How does the OUTBUF enable pin work on the TRF3761?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
How does the OUTBUF enable pin work on the TRF3761?
Hello,
Pin 1 is PD_OUTBUF. From the EVM schematic and datasheet, this pin is a software selectable input.
This means that if you are controlling the PD_OUTBUF using SPI (software), the pin will have no impact on actual performance.
If you need VERY fast on/off speed, you can use the pin to control the enable. Most applications do not require this.
By default, the software is configured such that the pin has no impact --- DB10 of register 0x0 is a "1". Important notice --- on the EVM, R37 (0ohm) will provide 3.3V from the SN74xx device causing the LED to be ON. Pulling this signal high or low with a jumper on W4 will have no impact on the output buffer (but the LED can be switched on/off).
Thanks!