I'm using TRF371125 for our product application. When studying the datasheet. There's no baseband EVM vs RF power and EVM vs frequency. We focus on 4 bands: a.750MHz b. 800MHz c. 1.8GHz d.2.6GHz When I measure the base-band EVM by using Agilent MXA and MXG. the base-band EVM is 3% when RF@2.6G, the base-band EVM below 2G is about 10%. Do you have any advice to solve this issue? B.T.W. Lo signal generate from TRF3765 and RFin use signal end to differential balun with 4.5M~3GHz compoment
Test steps:
1.Using TRF371125 on our Rx part key component.
2.Using TRF3765 to generate the Lo signal
3.Using Agilent MXG to generate the RF signal
4.Using Agilent MXG to measure the demodulated base-band EVM
5.RF signal@2.6GHz, Lo@2.6GHz=>base-band EVM~3%
6.RF signal@1.8GHz, Lo@1.8GHz=>base-band EVM~6%
7.RF signal@800MHz, Lo@800MHz=>base-band EVM~10%
8.RF signal@700MHz, Lo@700MHz=>base-band EVM~12%
9.RF using signal to differential balun (4.5MHz-3GHz)
10. lower band has the phase error, is there any register can compensate?