Hi,
I comprehend TRF37T05 is IQ Modulator for TDD.
However,I could not find the difference between TRF3705 and TRF37T05 in their data sheet.
Please tell me their performance comparison.
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kato-san,
The TRF37T05 is optimized for TDD application where the device can be powered down to save power during transmission off time. With power down mode enabled, the TRF37T05 only has a fraction of chip powered down (while the TRF3705 has the whole chip powered down). The partial power down allow less temperature change in TRF37T05 and better adjusted carrier feedthrough reponse which is need in TDD application.
The TRF37T05's power down current is 146mA, while the TRF3705's power down current is 35mA.
For TDD carrier feedthrough transient response performance of the TRF37T05, please refer to the following app note:
http://www.ti.com/lit/pdf/slwa074
If the application is not TDD and does not require good carrier feedthrough response over TDD switching, then TRF3705 and TRF37T05 have the same performance in general and can be used interchangeably.
-Kang