This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

phase detector for 160 MHz IF

Other Parts Discussed in Thread: LMX2492
hi,
i need to measure the phase difference (0 to 360' ) between two 160 MHz signals without use of digital clock or signals. i was planning to use AD8302 (analog devices) i am not happy with phase accuracy and i will have to use two for 360' phasedetection. i need an alternative IC which can indicate phase difference in terms of analog voltage. phase accuracy i require is +/-2' or better. can u suggest any IC from your side or if betteer recommnend circuit.