Other Parts Discussed in Thread: TRF370315, DAC908, TRF3705
Hello everybody, I would like to use the DAC908 (one for I and one for Q) as BaseBand inputs for the TRF370315.
At the very beginning I was thinking to ac couple the two devices in order to interface them (different common mode), but I studied a bit more and I found that TI has released a full resistive configuration in order to interface TRF370315 with DAC56x2.
TI also released a simple xls file (slwc083) usefull to find the correct values to interface the modulator with the DAC56x2.
I would like to know:
1) If I can use this configuration also for the DAC908
2) If the values I inserted in the xls file (and reported below) are correct
3) If there is a better solution to interface the two devices
4) If there are drawbacks I did not think about
Thank you