It looks like the FOM for the LMX2492 device is incorrect when selecting it (-215.8dBc/Hz instead of -227dBc/Hz). How can I correct this? There is an option to import a "noise file" in text format, but I am unsure of the format.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thomas,
I found this error and fixed it.
I am releasing a newer version of the PLLatinum Sim this week with this fix and several other upgrades.
One of the upgrades is related to the inport/export feature, as the current version is not consistent if the offset is in Hz or kHz. New version is consistent.
The format is:
offset, noise
you can separte with comma or tab and then put a new line after it. To do this, just do it in excel and save as tab-delimited text.
Regards,
Dean
Thanks Dean. I see the current version for download is still 1.1, released on 18 April 2016. Any idea when the newer version will be available?