This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gc5016 transceiver mode

Hello everyone,

Can I use channels AB as receiver and channels CD as transmitter in transceiver mode??

Thanx

Ahsan

  • Hello Ahsan,

    We do not have any tested configurations that work in this mode.  The configurations that have been used by customers for transceivers are:

       Channel AB - split IQ, one channel transmit, Channel CD - split IQ, one channel receive

       Channel AB - two channel transmit, Channel CD - two channel receive.

       two parts (TSW4100 EVM)

        one part DDC

        one part DUC

    Note: the GC5016 SEK can be used to test a transceive configuration with a special procedure.  The GC5016 can only be set in DDC or DUC mode,

    A special RevA GC5016 plug in board is required, and a special configuration is loaded.

     The transceiver configurations examples are included with the configuration description on the TI website:

    http://focus.ti.com/docs/prod/folders/print/gc5016.html

    See the GC5016 Configuration Guide.

    Regards,

    Radio Joe