This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About VCO range of LMX2571



Hello,to whom it may concern,

The fvco is 4300MHz~5376MHz in the datasheet(p6).




But Approximate VCO Ranges is 4200MHz~5520MHz in the datasheet(p42).



Which is correct of p6 and p42?

Best regards,

Manabu Ito

  • Hi Manabu,

    The Frequency range for the VCO is 4300MHz-5376MHz.

    Best Regards,

    Julian

    If my post answers your question, please click on "Verify Answer" button.

  • Hello Julian-san

    Thanks for your quick response!

    Sorry,I have one more question.
    How should I understand about Approximate VCO Ranges?
    Is this value only advisoly?

    Best regards,

    Manabu Ito
  • Hi Manabu

    Table 40 shows approximate VCO values. They may vary slightly in different devices.

    While the table shows 4200-5520 MHz, the actual VCO frequency range has to be wider in order to guarantee VCO frequency range is between 4300M – 5376MHz.

    We can only guarantee that the device will work on the  4300MHz-5376MHz range as shown in the Electrical Characteristics table.

    Thanks,

    Julian

    If my post answers your question, please click on "Verify Answer" button.

  • Hi Julian,

    when looking on the single VCOs, what would be a safe, guaranteed range? This information would be important for us because we will have a detailed design in which we want to choose VCOs directly.

    data sheet values:
    VCO Core Typ. Freq. Range (MHz)
    VCOL: 4200-4700
    VCOM: 4560-5100
    VCOH: 4920-5520

    Could this the be the safe range?
    VCOL 4300-4640
    VCOM 4640-5000
    VCOH 5000- 5375

    Absolute values are necessary for us because the overlapping range of the VCOs result in different overall settings which must be calculated precisely.

    Thanks,
    Alex
  • Any advice? Or do I have to open a new thread, because this one has been marked as "answered" before?