Hi,
When configuring the LMX2571 the PFD_DELAY_F2 (table15) has a significant effect on the phase noise and spurs.
Q1. Can anybody describe what these bits are doing? PFD_DELAY_F2 in table 15.
Q2. Setting these these bits I can potentially get a lower phase noise. Does this have an impact on anything else?
Q3. Can I use them out of the recommended range if I get a lower noise? If not why not?
I ask Q1-Q3 since the operation/function of the PFD_DELAY_F2 is not well described.
Thanks all.