This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF3722: SPI Timing Diagram - Figure 131

Part Number: TRF3722


Hello there,

My customer is working on a SPI control module in Verilog for the TRF3722 but are having some troubles deciphering the timing diagrams in the datasheet as there are a couple graphic issues where text overlays and looks jumbled. Do we have a clearer timing diagram on the 4WI Timing Diagrams or any added documentation for them to reference as they work with this device?

Appreciate your help and direction,

-Amanda

  • Hi Amanda,

    Let me look into this.

    Regards,

    -Oscar

  • Amanda:

    The timing diagrams are shown in Figure 130 and 131 of the datasheet.  On my end I do not see any graphics issues related to text overlays or jumbled text.  This may be a function of the pdf viewer being used.  You may also try to view timing diagrams in related devices like the TRF3720 or TRF3711 where the SPI timing structure is the same.

    A copy of figure 131 is below.  I will close this post.  If there are further questions please feel free to post a new thread.

    --RJH