This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW38J84EVM: TSW38J84EVM

Part Number: TSW38J84EVM
Other Parts Discussed in Thread: TRF3722

I would like to use the FMC connector to provide SPI control of the TRF3722.  The FMC connector has signals listed as FMC_B5 and FMC_B6, but there is no description of these signals that are provided to the CPLD on the TSW38J84EVM. 

My questions are; are these signals usable for SPI control of the TRF3722?

Is there any information on the CPLD such that I can configure the CPLD to provide SPI control of the TRF3722?

Please let me know.

Thanks,
Troy Robinson

  • The CPLD was primarily intended to serve as a pass-through, voltage translator to the programmed devices on the board. There is no available information for using it as a programming device nor using the FMC connector as the programming path. --RJH