Hi dear supporting team,
customer has below questions on TRF3722, need double check with you:
1. in d/s, there is only max input ref of 350MHz, what's the minimum frequency input? could it accept 10MHz?
2. if do not use LO_OUT, could it be floating?
3. for the ferrite bead of the power supplies, should customer add them all? and how to select the value of ferrite bead?
tks a lot!