Part Number: ADC31RF80
Team,
Customer has issue to access digital SPI bank(analog SPI bank is OK) no matter to read 02h - 04h or to next 4 pages. Would you please have a look below commends and let us know if any comments? Thanks.
ADC32RFxx_LOWLEVEL
0x0012 0x04 // write 4 to address 12 page select
0x0000 0x81 // software reset
0x0012 0x00
0x0011 0xFF // write to address 0x0011 ADC page select
0x0022 0xC0
0x0032 0x80
0x0033 0x08
0x0042 0x03
0x0043 0x03
0x0045 0x58
0x0046 0xC4
0x0047 0x01
0x0053 0x01
0x0054 0x08
0x0064 0x05
0x0072 0x84
0x008C 0x80
0x0097 0x80
0x00F0 0x38
0x00F1 0xBF
0x0011 0x00 // Set 0x0011 with 0x00 to enable only master page later
0x0012 0x04 // write 4 to address 12 page select
0x0058 0x20 // SYNC polarity inverted as the hsdcpro.ini inverts the sync
0x0025 0x01
0x0026 0x40
0x0027 0x80
0x0029 0x40
0x002A 0x80
0x002C 0x40
0x002D 0x80
0x002F 0x40
0x0034 0x01
0x003F 0x01
0x0039 0x50
0x003B 0x28
0x0040 0x80
0x0042 0x40
0x0043 0x80
0x0045 0x40
0x0046 0x80
0x0048 0x40
0x0049 0x80
0x004B 0x40
0x0053 0x60
0x0058 0x20 //Toggle inverse Sync to on (ini must also have isync = 1)
0x0059 0x02
0x005B 0x08
0x0062 0xE0
0x0065 0x81
0x0066 0x80 // increase JESD swing, 00 default, 80 max
0x006B 0x04
0x006C 0x08
0x006E 0x80
0x006F 0xC0
0x0070 0xC0
0x0071 0x03
0x0076 0xA0
0x0077 0x0A
0x007D 0x41
0x0081 0x18
0x0084 0x55
0x008A 0x41
0x008E 0x18
0x005c 0x07
0x0012 0x00 //master select 0x00
0x0011 0xFF
0x0083 0x07
0x005C 0x01
0x0011 0x00
0x0012 0x00 //master select 0x00
0x5000 0x01 // DDC enable CHA
0x5001 0x05 // DDC by 12 CHA
0x5002 0x01 // Two bands CHA
0x5007 0x10 // LSB NCO1 1890 MHz CHA
0x5008 0xA4 // MSB NCO1 1890 Mhz
0x5009 0x00 // LSB NCO2 1.75Ghz
0x500A 0x00 // MSB NCO2
0x500B 0x85 // LSB NCO3 1.78Ghz
0x500C 0x9A // MSB NCO3
0x500D 0x92 // DDC1 LSB NCO 1.99Ghz
0x500E 0x93 // DDC1 MSB NCO
0x5014 0x01 // 6dB DDC0
0x5016 0x01 // 6dB DDC1
0x5800 0x01 // DDC enable CHB
0x5801 0x05 // DDC by 12 CHB
0x5802 0x01 // Two bands CHB
0x5807 0x10 // LSB NCO1 1890 MHz CHB
0x5808 0xA4 // MSB NCO1 1890 Mhz
0x5809 0x00 // LSB NCO2 1.75Ghz
0x580A 0x00 // MSB NCO2
0x580B 0x85 // LSB NCO3 1.78Ghz
0x580C 0x9A // MSB NCO3
0x580D 0xe8 // DDC1 LSB NCO 1.78Ghz
0x580E 0x97 // DDC1 MSB NCO
0x5814 0x01 // 6dB DDC0
0x5816 0x01 // 6dB DDC1
0x4001 0x00
0x4002 0x00
0x4003 0x00 //channel A
0x4004 0x68
0x6044 0x60 // Loop EN1
0x6068 0x40 // Loop EN2
0x60A2 0x09 // nyquist zone = 2
0x4003 0x01 // channelB
0x4004 0x68
0x6044 0x60 // Loop EN1
0x6068 0x40 // Loop EN2
0x60A2 0x09 // nyquist zone = 2
0x608D 0x50 // IMD3 correction
0x608B 0x05 // IMD3 correction
0x6000 0x00 //clear reset
0x7000 0x00
0x6000 0x01 //reset digital
0x7000 0x01
0x6000 0x00 //clear reset
0x7000 0x00
0x4003 0x00
0x4004 0x69
0x6002 0x01 // set JESD mode0 = 1
0x7002 0x01 // set JESD mode0 = 1
0x6037 0x00 // PLL MODE = 20x
0x7037 0x00 // PLL MODE = 20x
0x6032 0x3C // set -6.2dB TX de-emphasis Lane 0, chA
0x7032 0x3C // set -6.2dB TX de-emphasis Lane 1, chA
0x6033 0x3C // set -6.2dB TX de-emphasis Lane 2, chA
0x7033 0x3C // set -6.2dB TX de-emphasis Lane 3, chA
0x6034 0x3C // set -6.2dB TX de-emphasis Lane 0, chB
0x7034 0x3C // set -6.2dB TX de-emphasis Lane 1, chB
0x6035 0x3C // set -6.2dB TX de-emphasis Lane 2, chB
0x7035 0x3C // set -6.2dB TX de-emphasis Lane 3, chB
0x6001 0x80 //EN CTRL K
0x7001 0x80
0x6007 0x0F //set K to 15
0x7007 0x0F
Regards,
Allan