This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7070: AFE7070: IO characteristics

Part Number: AFE7070


While designing a board for the AFE7070, I came across multiple issues:

  • Does the LVDS_P/_N output, if unused, need to be terminated?
  • If LVDS output isn't used at all, does LVDSVDD18 need to be
    • connected to 1.8 V?
    • decoupled separately?
  • The maximum currents
    • I_IOVDD,
    • I_CLKVDD18,
    • I_DACVDD18,
    • I_LVDSVDD18 and
    • I_DACVDD33
      are inconveniently unspecified in the datasheet table on p.5.
      Can a maximum supply current for these be clarified?
      This is kind of central to power supply design in low-power mass application.
  • In Dual Input Clock Mode, it seems that DACCLK_P and CLK_IO can be identical, in which case the data lines should be changed and finished changing in the negative period of DACCLK_P=CLK_IO. Is that correct?
  • Optional: Does the RFOUT pin withstand operation without load (i.e. with an impedance mismatch -> infinity)?
  • Optimally: Is there a mode which allows an RF signal path test during manufacturing, and if so, how to access it and what LO/clock would have to be supplied?

Thank you in advance,

Marcus Müller