Part Number: TRF370417
Other Parts Discussed in Thread: DAC3484, DAC38J84, TRF3705, DAC5687, DAC5688
To whom it may concern,
According to the data sheet, TRF370417's two BB inputs have single-ended input impedance of 5kOhm.
I wonder if the differential input impedance is 100ohm.
If the BB inputs are high impedance, then why doesn't the TRF370xEVM have any 50ohm termination at the BB input ports?
Please help.
Best,
Weiyu