Hi All,
I have a Spring helical Antenna of 433 MHz, when I measure it's S11 while connecting directly on port of Network Analyzer at 433 MHz i get
S11 value : -19 dbm.
VSWR : 1.2
and a complex value of 32 -j10 on smith chart.
Ques : Now my first query is After placing my antenna on Board how should i measure it ?
The way i tried is, I used an coaxial cable of 70 cm and calibrate it to end. then i solder it on the starting point of matching network.
But the antenna parameter values got changed.
Ques: Is this the correct way of doing it?
Ques: Do i have to make antenna 50 Ohm using smith chart and matching circuit? Or just good S11 and VSWR are sufficient?
Ques: How should i approach the antenna tuning on my board and verify it whether its correct or not?
I am totally new to all this and i would appreciate any guidance towards right approach
Thanks