I have included in my design the LMX2594 Synt.
I would like to implement a Balun (attached pdf) by taking two LMX2594 RF outputs and achieve single ended output that will provide me about 7dBm output power instead of 2dBm @ 13GHz
I consider to use Balun because I'm afraid to use the pull–up with inductor solution due to 50 ohm impedance that might be impaired (according to LMX2594 datasheet) (are there 1n inductors that are good for 13GHz if yes can you recommend?)
The thing is that in the datasheet such solution is not mentioned thus I wonder if its feasible/recommended ? if yes can you provide some typical recommendation for such solution?