This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Luck Wu,
Is the customer planning to use a differential signal as input?
In the design above, differential signal can be used as input to J2 (INP) and J1 (INM).
The following changes had to be made to enable differential input:
1. Remove T1 and T2
2. Populate C414, R1, C1, C415, R11 and C6.
Regards,
Vijay
Hi Lian,
Hardware reset is required for the device before loading the configuration. Please connect it to FPGA / ASIC.
It's not necessary to connect GPIO4. It can be programmed as CMOS SYNCB. But I see customer has connected LVDS SYNCB.
I see GPIO 1, 2 and 3 are connected. If customer is not planning on using NCO switching, those don't need to be connected as well.
Regards,
Vijay