We would like to do some experiments with millimeter waves (mm-waves). We have experience with software defined radios (SDRs) with center frequencies between 60Mhz to 6GHz, such as USRP B and X series, AD9361, AD9371, hackRF, etc. Our question is whether there is any development board, or general purpose SDR, with features and capabilities similar to SDRs mentioned above, with which we could set up a system and start transmitting and receiving signals with center frequencies preferably around 60GHz.
Basically, what we are looking for is a setup where we can feed our custom baseband signals (IQ data that we construct, in complex-float, complex-int, or complex-short format) over 60GHz band, and receive the baseband IQ data on the other side.