Dear Sir,
I would like to get some clarifications with regard to the evaluation of the GC5325SEK. We had got the the four upgrades to the board (DSP and GUI software, FPGA firmware and the DSP Weuffen USB UHPI interface board) in November 2010. Subsequent to the upgrades, I could do the loopback test successfully. I also tested the GC5325SEK with an external PA (AH101) and observed an improvement in ACPR. Currently, I am in the process of evaluating the GC5325SEK with an external PA of higher power capability.
1. We would like to evaluate the performance of the GC5325SEK for narrowband signals. I recall from the conversation I had with Mr Joe Quintal during the TI Wireless Infrastructure Seminar in Bangalore on Oct 21,22 2010 that you had tested the GC5325SEk with Multicarrier GSM. The files for the same have been included in the folder named "basedband data" in the installation folder. I could not find any information regarding the evaluation of GC5325SEK for Multicarrier GSM. Could you please give us the configuration you had used while evaluating the GC5325SEK for Multicarrier GSM and the test results ?
2. Regarding the CLK for the GC5325SEK, it has been stated in the document that the clock must be between 650 and 750 MHz. What is the reason behind this constraint ?
3. I have been using LO frequencies in the range 700 - 1400 MHz. The mixer being used is HMC483MS8GE. The LO drive level specified in the data sheet of HMC483MS8GEis -4 to +4 dBm. It has been stated in the document that the LO power should be set approximately to -7 dBm when using this configuration. Cal Feedback could not be successfully done when I set the LO drive level to -7 dBm.On contacting the TI local support in Bangalore, I was told to set the drive level of LO_IN to +7 dBm for doing the loopback test. I observed that the power level of RX_MIX_LO was + 10.69 dBm for a LO drive level of +6 dBm. It is certainly out of the recommended LO drive level for the HMC483MS8GE. What could possibly be the issue here ?
Please do get back to us at the earliest.
Regards,
Prem Krishnan
Senior Staff Scientist,
Broadcast & Communications Group,
Centre for Development of Advanced Computing (C-DAC),
Vellayambalam, Trivandrum -695033.
Kerala, India.
Tel: +91 - 471 - 2723333 (Ext: 354)Mob: +91 9846433239