This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AN099 code issue



I have a project about transmitting audio signals using CC1110 and Codec AIC3104 according to TI's reference. However, due to the incorrect code (swra368 ), when I used the RTL SDR to receive the signal, it did not receive the audio signal but only the waveform, I measured the RX signal from the codec and still got the normal output signal. I look forward to its code support.

  • Hi Nguyen,

    If re-building the project then I recommend that you make sure to use the same IAR version (EW8051 v5.4) and compiler that was used to develop this application note.  Otherwise, no further support can be provided for such a deprecated solution.

    Regards,
    Ryan