Part Number: DAC38RF80
Other Parts Discussed in Thread: DAC38RF82
We are planning to use multiple DAC38RF80. I've read thru datasheet sections 8.3.9, 8.3.10 on the multi-Device synchronization. How does that work when the DUC and internal DAC clock PLL are used. It appears the DUC can be synchronized using SYSREF, but I don't see a detailed explanation of how it works. Also, how is the internal PLL synchronized, in order to repeatably phase align its output.
Note: for our application, the SYSREF signal and lower frequency input DACCLK signal (~250MHz) will be generated by using a high quality JESD204B clock generator. We'll be using 8x or 12x interpolation in the DAC38RF80, and the internal DAC clock will be minimum of 6GHz.
thanks,
Scott