I'm looking for a single channel transmit and receiver mm-wave radar module 77 GHz of 60 GHz. I'm interested if the TI radar modules be used as a stepped frequency(SF) CW radar. It's clear that they operate as FMCW with a continual sweep, but can they be operated in a stepped frequency mode? In the stepped frequency(SF) mode, the frequency of the radar is changed in discrete steps. At each step the radar has a fixed frequency and a short time is made for the system to settle. Then a measuremnet of phase and amplitude is made (or I & Q if you like), before moving to the next frequency. However, for the system to be used as a SFCW radar the signal paths all the way to the ADCs have to be DC coupled. In standard FMCW systems AC coupling is normally used. So the question to you is can they be operated as a SFCW radar with a DC signal coupling to the ADCs? many thanks, Neil Salmon