Part Number: LM15851
Hi!
I have some questions regarding LM15851 initialization.
1. Does SPI_RES (POR register) supersede SWRST (CFGA register). I.e. SPI_RES resets the whole chip (including internal state machines, etc.), and SWRST resets register's content only. Is it correct?
2. Should I give the chip some time after issuing the SPI_RES command to get the chip reset before I could issue another command or could the next command be issued immediately after the reset?
3. In JESD204 Startup Sequence (8.3.1, p. 75), when programming JESD_EN = 0, then CAL_SFT = 1, and then JESD_EN = 1, should some delays be inserted between these commands to give them time to be executed, or could the commands be issued side by side without any delay?
Please, describe the initialization process in some more details then it described in the datasheet.
Best regards,
Victor.