Hi everyone,
We are working with TRF372017 IQ modulator on our custom board and are currently trying to program the seven registers in it for a modulated output of 2450 MHz. Looking at the modulator's data sheet, we expect, for a divider value of 2 from VCO output to RF mixers input and divider value of 1 from VCO output to the tap provided, we should see 4900 MHz at the VCO tap output. Our reference clock is 30 MHz and can be changed, if required. Following is the schematic for reference.
Can someone suggest what is the sequence in which the registers need to be programmed and what are the optimized values for all seven registers, to obtain modulated output of 2450 MHz?
Also, what are the status registers available and how to read their values? For example, the PLL lock status? If someone can respond, that would be helpful too.
-Chan100