Part Number: TPS2115A
Hello,
if IN1/IN2 voltage one of them are 0V or floating, TPS2115A still work normal to switching input voltage to output? Thank you.
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2115A
Hello,
if IN1/IN2 voltage one of them are 0V or floating, TPS2115A still work normal to switching input voltage to output? Thank you.
BR
Patrick
Hi Patrick,
Yes, the TPS2115A will still work as long as one of the supplies is greater than 2.8V. For example, if IN1=5V and IN2 is disconnected, then the part will still be able to pass IN1 to the output. It is not recommended to switch to the disconnected (or 0V) supply to power the output.
Thanks,
Alek Kaknevicius