Part Number: IWR1642
Other Parts Discussed in Thread: , TIDEP-0090, AWR1642BOOST
The "ES2.0 Sticker On the PCB" as denoted by 8244.IWR1642-ES1.0-to-ES2.0-transition.pdf is NOT Present.
How can I tell if it is an IWR1642A?
The chip is marked:
YN
TM4C129
4NCPDTT3
81COOTKW
G4
The CHIP itself does NOT have ANY Marking “IWR1642” at all, no matter what the revision
The EVM Just Delivered Does Have Two Stickers: 5337900083 and IWR1642BOOST with NO Mention of Revision or ES number.
I need the Latest Version that will work with the 2.0 Software in order to get the Best Tracking and Clustering for which TIDEP-0090 was recommended on E2E and I am anxious to try it out.
I already have an AWR1642BOOST and an IWR1642BOOST but both are ES1.0
What did I just receive?
I hesitate to power it up, flash it or do anything other than look at it as it may need to be returned.
Please advise, Thank You, Dan