This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: BOOST Just received from the TI Store Does NOT indicate if it is ES2.0 or Rev A

Part Number: IWR1642
Other Parts Discussed in Thread: , TIDEP-0090, AWR1642BOOST

The "ES2.0 Sticker On the PCB" as denoted by 8244.IWR1642-ES1.0-to-ES2.0-transition.pdf is NOT Present.

How can I tell if it is an IWR1642A?

The chip is marked:

YN

TM4C129

4NCPDTT3

81COOTKW

G4

The CHIP itself does NOT have ANY Marking “IWR1642” at all, no matter what the revision

The EVM Just Delivered Does Have Two Stickers: 5337900083 and IWR1642BOOST with NO Mention of Revision or ES number.

I need the Latest Version that will work with the 2.0 Software in order to get the Best Tracking and Clustering for which TIDEP-0090 was recommended on E2E and I am anxious to try it out.

I already have an AWR1642BOOST and an IWR1642BOOST but both are ES1.0

What did I just receive?

I hesitate to power it up, flash it or do anything other than look at it as it may need to be returned.

Please advise, Thank You, Dan