This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM56: Schematic reivew

Part Number: LM56

Dear team

There is a good news that we design in LM56 in customer's new project, but meet some questions on LM56.
For verification, set T1=10℃ T2= 46 ℃. R1=10k ohm, R2=4.7k ohm,R3=12.1k ohm.
But at room temperature 25℃, both two out1 and out2  are low.
Could you help this question?

 The schematic as below

many thanks

Denny