-
I have an urgent project need right now, It is required that the power on start time of 1843 can be within 100ms, and the power on time here is mean of when IWR1843 in the offline status ,from the power supply to the serial port output the first frame of 1DFFT data.However, I have reduced the power on time from 400ms to 200ms for the out of box project. I don't know where I can continue to make modifications to reduce the boot time.
-
Another requirement is how to reduce power consumption. I need the 1843 to go into low power state, If this configuration is available, please let me know the details. In working condition of 1RX,1TX, what is the lowest power consumption.
- Best regards,
- Hope to hear from you soon.
Lucky