Other Parts Discussed in Thread: AWR1642, DCA1000EVM
When I open mmwave studio,I don't see radar API.Here are the environment:
1)CCS 10.3 installed as the default path
2)Matlab Runtime 8.5.1 32bit
3)FTDI,download the corresponding file from the official website and update it manually in device manager. And I can see this when I plug in the awr1642.
4) VS code 2019, with
5) mmwave studio is 2.1 and the OS is windows 10.
6) RadarLinkDLL.dll is already in the folder, it's so strange that the mmwave studio can't load it.
I want to use the mmwave studio to capture raw data from awr1642, and that EVM is all I have.