Hi,
Im trying to figure out how to insert my written code into a selfmade board using a PGA970QPHPR. Im using the XDS200 JTAG Emulator which has a 10 pin adapter to match the EVM board but just 1 seems to be connected. Pin 1 and (2+4) of the XDS200 are connected to SWDIO and SWDCLK of the PGA. I thought of replicating such a connection in order to load the code onto the chip.
Is there a pinnout of the connecter J22? Also is there any workaround to CodeComposerStudio, I would like to use my own IDE...
Regards Paul