The wireless temperature sensor, which uses the TMP117, wants to calibrate the temperature accuracy of each sensor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The wireless temperature sensor, which uses the TMP117, wants to calibrate the temperature accuracy of each sensor
yongxian Fan,
Which wireless temperature sensor are you referring to?
All temperature sensors from TI are calibrated by TI in production in order to meet the datasheet specifications. Most customers do not calibrate.
thanks,
ren
Links链接:https://pan.baidu.com/s/1bcuS1grFBdnp5llbBSuHGQ Extraction Code提取码:zrvu
The above is the legend information of wireless temperature sensor.We want to calibrate the temperature accuracy of this equipment.However, the cryogenic section, such as the temperature point of-20 °C, can not be calibrated by placing it in the coolant of the thermostatic tank.I hope there are other good proposals.
Dear Yongxian -
The link you sent over is a blocked site for us. Please attach your system requirements for Ren to look at, if possible, using the insert dropdown in E2E - if this is not possible, please respond with a list or table. The TMP117, as Ren said, comes from TI already calibrated, and the accuracy for various temperature ranges are given in our datasheet, which you should be able to easily duplicate by following the placement recommendations in same.