This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: bpmCfg command

Part Number: AWR1843
Other Parts Discussed in Thread: AWR1642

Hi, the SDK users guide 3.5.0.4 says this:

BPM enabled:
If BPM is enabled in previous
argument, this is the chirp index for
the first BPM chirp. It will have
phase 0 on both
TX antennas (TXA+ , TXB+). Note
that the chirpCfg command for this
chirp index must have both TX
antennas enabled.

so:

bpmCfg -1 1 0 1 means that both chirps will be transmitted with two antennas simultaneously with 0 phase between txa and txb in the first chirp and phase 180 in the second chirp?

and

BPM disabled:
If BPM is disabled, a BPM disable
command (set phase to zero on
both TX antennas) will be issued
for the chirps in the range
[chirp0Idx..chirp1Idx]

so:

bpmCfg -1 0 0 0 means that both chirps will be transmitted with two antennas simultaneously with 0 phase between txa and txb for the chirps in the range [chirp0Idx..chirp1Idx]?

  • Hi Jairo,

    I would need a couple of days to get this information, let me get back to you by Friday.

    Regards,

    Aayush

  • Hi, do you have any info about this question?

  • Hi Jairo,

    Sorry I took so long for this information.

    bpmCfg -1 1 0 1 means that both chirps will be transmitted with two antennas simultaneously with 0 phase between txa and txb in the first chirp and phase 180 in the second chirp?

    This is correct*.

    bpmCfg -1 0 0 0 means that both chirps will be transmitted with two antennas simultaneously with 0 phase between txa and txb for the chirps in the range [chirp0Idx..chirp1Idx]

    This is also correct*.

    You can have a look at the MmwDemo_bpmConfig function in the demo source code to see the behavior of the demo when bpmCfg is disabled/enabled. This function is always called by the 16xx demo, so one of the two bpm config (enabled or disabled) paths must be executed.

    *The caveat here is the 'simultaneous' part of your statement. bpmCfg in itself does not configure the transmitters to transmit simultaneously. This is done by the last argument of the chirpCfg command. So, the assumption in your statement is that the chirps are set up to use the TXs simultaneously. I just wanted to highlight this as in the TDM usage of the OOB demo, you will find a  "bpmCfg -1 0 0 1" command, but the chirps are configured in a one TX at a time fashion, so you won't find that multiple transmitters are transmitting with 0 phase difference as you mentioned in the second statement.

    Regards,

    Aayush

  • I also want to add that the semantically correct usage of what you are trying in the second case would be "bpmCfg -1 0 0 1", which formally affects chirps 0 and 1. "bpmCfg -1 0 0 0" only affects chirp 0, however, the chirps have a 0 phase by default to begin with, so it would probably end up having the same effect.

    Regards,

    Aayush

  • bpmCfg in itself does not configure the transmitters to transmit simultaneously.

    I do not understand why do you say that, the SDK user guide says:

    from SDK guide:

    bpmCfg

    BPM MIMO configuration.
    Every frame should consist of alternating chirps with
    pattern TXA+TxB and TXA-TXB where TXA and
    TXB are two azimuth TX antennas.

    This is alternate
    configuration to TDM-MIMO scheme and
    provides SNR improvement by running 2Tx
    simultaneously.

    so I understand that when I set 1 in the second parameter of the bpmCfg command I am enabling  2 tx simultaneously

    This is done by the last argument of the chirpCfg command.

    Ok I agree with this because the SDK guide talks about it:

    BPM enabled:
    If BPM is enabled in previous
    argument, this is the chirp index for
    the first BPM chirp. It will have
    phase 0 on both
    TX antennas (TXA+ , TXB+). Note
    that the chirpCfg command for this
    chirp index must have both TX
    antennas enabled.

    but, if the guide mentions the chirpCfg command inside the bmpCfg command I understand that both commands depend on each other to enable the tx simultaneously, I mean, ok I need the last argument of the chirpCfg command but I also need to set 1 the second argument in the bpmCfg command, is this right?

    I also want to add that the semantically correct usage of what you are trying in the second case would be "bpmCfg -1 0 0 1", which formally affects chirps 0 and 1. "bpmCfg -1 0 0 0" only affects chirp 0, however, the chirps have a 0 phase by default to begin with, so it would probably end up having the same effect.

    I don´t understand this, could you explain it better, please?

    thanks

  • bpmCfg -1 0 0 0 means that both chirps will be transmitted with two antennas simultaneously with 0 phase between txa and txb for the chirps in the range [chirp0Idx..chirp1Idx]

    This is also correct*.

    So according to what you have explained to me, this is no correct, bpmCfg -1 0 0 0 does not mean that I am tx simultaneously even if I have both tx enables in the chirpCfg command, so I have understand this:

    here I enable 2tx simultaneously (BPM mimo) because I set the same 3 antennas in both chirps and enable the bpmCfg command

    chirpCfg 0 0 0 0 0 0 0 3
    chirpCfg 1 1 0 0 0 0 0 3
    bpmCfg -1 1 0 1

    here I enable TDM mimo because I set the same different antennas in both chirps and bpmCfg command is disabled

    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 2
    bpmCfg -1 0 0 1

    I think this would not be a valid config:

    here I enable 2tx simultaneously because I set the same 3 antennas in both chirps but I am disabling the bpmCfg command, so if I disable bpmCfg I am trying to do TDM mimo, but TDM mimo uses different antennas for each chirp so this is a contradiction

    chirpCfg 0 0 0 0 0 0 0 3
    chirpCfg 1 1 0 0 0 0 0 3
    bpmCfg -1 0 0 1

    what do you think?

  • Hi Jairo,

    Let me start over with the explanation.

    The chirpCfg is solely responsible for which antennae are enabled for a particular chirp. bpmCfg has a role to play to enable BPM as well, but it is not needed to enable multiple transmitters. bpmCfg just sets the phase shift of the antennae (it programs the phase shifters in the RF via mmwavelink). So, it is assumed that chirpCfg will take care of enabling the transmitters, and bpmCfg can then set the phase shifts for them. bpmCfg is applied in MmwDemo_bpmConfig via a call to MMWave_addBpmChirp, which takes rlBpmChirpCfg_t as an argument.

    MmwDemo_bpmConfig calls MMWave_addBpmChirp twice, once for chirp 0 (setting TX phases to 0, 0 degree) and once for chirp 1(setting TX phases to 0, 180 degree).

    Definition of rlBpmChirpCfg_t:

    typedef struct rlBpmChirpCfg
    {
        /**
         * @brief  Chirp Start Index, Valid Range 0 -511
         */
        rlUInt16_t chirpStartIdx;
        /**
         * @brief  Chirp End Index, Valid Range from chirpStartIdx to 511
         */
        rlUInt16_t chirpEndIdx;
        /**
         * @brief  b0  CONST_BPM_VAL_TX0_TXOFF \n
                         Value of Binary Phase Shift value for TX0, when during idle time \n
                         b1  CONST_BPM_VAL_TX0_TXON \n
                         Value of Binary Phase Shift value for TX0, during chirp \n
                         b2  CONST_BPM_VAL_TX1_TXOFF \n
                         Value of Binary Phase Shift value for TX1, when during idle time \n
                         b3  CONST_BPM_VAL_TX1_TXON \n
                         Value of Binary Phase Shift value for TX1, during chirp \n
                         b4  CONST_BPM_VAL_TX2_TXOFF \n
                         Value of Binary Phase Shift value for TX2, when during idle time \n
                         b5  CONST_BPM_VAL_TX2_TXON \n
                         Value of Binary Phase Shift value for TX2, during chirp \n
                         b15:6 Reserved \n
         */
        rlUInt16_t constBpmVal;
        /**
         * @brief  Reserved for future
         */
        rlUInt16_t reserved;
    }rlBpmChirpCfg_t;

    As you can see, this structure only contains information about the phase shift of various TX. It will set phase shifters for different TX to either 0 degree or 180 degree.

    When bpmCfg is enabled, for a start and end index of chirp, MmwDemo_bpmConfig function populates this structure (once for each chirp) for the antennae to have the appropriate phase needed for BPM. When disabled, it still registers the BPM config, but with 0 degree phase for all TX (which has no effect as profile config already sets the phase shift of all antennae to 0 in OOB demo).

    Your understanding of all three configs you listed in your last reply is correct. The first two configs are valid, the third one is invalid for the OOB demo. Note that the device itself has no issues with having multiple transmitters enabled at any phase for any chirp, but there are processing constraints in place which render the third configuration invalid for the OOB demo.

    Now, for this statement:

    I also want to add that the semantically correct usage of what you are trying in the second case would be "bpmCfg -1 0 0 1", which formally affects chirps 0 and 1. "bpmCfg -1 0 0 0" only affects chirp 0, however, the chirps have a 0 phase by default to begin with, so it would probably end up having the same effect.

    The proper usage of bpmCfg in the disable case should be "bpmCfg -1 0 0 1". "bpmCfg -1 0 0 0" is technically incorrect if two chirps are set up, but I think it would still work. This is because the purpose of this command in the disable case is to set the TX antenna phase shifts to 0. But, profile configuration already does this for all chirps. So "bpmCfg -1 0 0 0" would set chirp 0's phase to 0 and omit chirp 1, but chirp 1's phase has already been set to 0 in its profile configuration.

    I hope that cleared up the role of bpmCfg a little.

    Regards,

    Aayush

  • Hi,

    bpmCfg has a role to play to enable BPM as well, but it is not needed to enable multiple transmitters

    So, is this an errata?

    from SDK guide:

    bpmCfg

    BPM MIMO configuration.
    Every frame should consist of alternating chirps with
    pattern TXA+TxB and TXA-TXB where TXA and
    TXB are two azimuth TX antennas.

    This is alternate
    configuration to TDM-MIMO scheme and
    provides SNR improvement by running 2Tx
    simultaneously.

  • Hi,

    I don't see an issue with the SDK documentation's statement. bpmCfg does indeed configure BPM enable/disable, and enabling BPM does have the overall effect of running 2TX, it's just that if BPM is enabled, chirpCfg needs to ensure that both TXs are enabled for the BPM chirps to be configured properly. 

    Regards,

    Aayush

  • Hi,

    Note that the device itself has no issues with having multiple transmitters enabled at any phase for any chirp, but there are processing constraints in place which render the third configuration invalid for the OOB demo.

    what are those processing constraints?

    How could I know if a lab is able to tx simultaneously?, e.g. the awr1642 oob lab does not mention that simultaneous tx could be enable, every time we generate a 2tx config we get something like this:

    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 2
    bpmCfg -1 0 0 1

    and in the bpm example you provide in awr1642 profiles in sdk 3.5.0.4, this:

    chirpCfg 0 0 0 0 0 0 0 3
    chirpCfg 1 1 0 0 0 0 0 3
    bpmCfg -1 1 0 1

    I never have seen an example where we have the same antennas configured in chirpCfg with bpmCfg disabled or even, without the bpmCfg, always the multiple antenna config is with bpmCfg to 1

    and always the chirpCfg with different antennas has bpmCfg to 0 (disabled) or no bmpCfg command, that is why I say that bpmCfg enables the simultaneous tx in addition to the phase of the chirps, of course, your document also mentions the same

  • Hi Jairo,

    what are those processing constraints?

    The processing constraints are exactly what you encountered. The OOB demo can only do two kinds of processing: either TDM-MIMO mode (different antenna being enabled at different chirps), or BPM mode (multiple TX enabled, but with a particular phase applied).

    What I said though was that the hardware can support multiple TXs at any arbitrary phase to transmit simultaneously. The transmitters would enable, and the raw data would be gathered in the ADC buffer as usual. However, the programmer would have to make sure though that this data is usable. The OOB demo shows just one such mode for multiple TXs being enabled: BPM mode. In the documentation you highlighted, the BPM config is responsible for the second half "... while still ensuring the separation of these signals".

    To give you concrete examples, our labs showcase two other modes where multiple TXs are enabled without using BPM (both use chirp config to enable multiple TX).

    You can have a look at the MRR lab (lab 7). For MRR 120m config, MRR enables all 3TX at the same time with 0 phase shift. This enabling is done by the macro CHIRP_MRR_0_TX_CHANNEL and CHIRP_MRR_1_TX_CHANNEL defined in the mrr_config_chirp_design_MRR120.h file. Both of these are used with the chirp config API to enable the transmission of multiple TX at the same time.

    Similarly, the MRR beamforming (lab 11) is an enhancement on the same concept. Apart from enabling all TX in the MRR mode with chirp config, it also applies phase shifts to the TX so that a beam is formed at a particular angle. Again, multiple TX are enabled by the chirp config API, and phases are applied via rlRfSetPhaseShiftConfig API. 
    I can see how the wording of the documentation is misleading, but the bpmCfg in itself does two things: configures the phase shifters appropriately, and configures the datapath for BPM mode.
    Regards,
    Aayush