In LHR mode, how do you set RPMIN if the sensor RP isn’t covered entirely by a single RPMIN setting as shown in Table 36.
- Our sensor is predicted to be: 2.01 kOhm <= Sensor Rp <= 7.07 kOhm.
- The 3kOhm setting covers 2.1 to 6.5 kOhm
- The 6kOhm setting covers 4.2 to 13.1 kOhm