The value of pfVcoSelect is 2 in the MMWAVELINK_CASCADE_EXAMPLE/mmwaveconfig.txt file from the mmwave DFP. In reading the radar interface control document for the corresponding API, I would have thought that the FORCE_VCO_SEL should be set to 1 (Forced external VCO selection) on the slave devices, but not on the master. I don't see anywhere in the example code where that happens, though. It looks like it's being set to 2, so FORCE_VCO_SEL=0, for all of the devices. Am I misunderstand the meaning of the FORCE_VCO_SEL field? If so, what are the circumstances where that field would ever need to be set to 1?
Thanks,
Dave