This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Max unambiguous detectable velocity upto 300 km/h

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi,

We are working on an "expressway traffic monitoring application",

The Maximum velocity measurement requirement is 200km/h plus

Currently, we are using IWR1642Boost for evaluation purposes. 

Referring to the document spyy002b.pdf Page number 7, there it is mentioned  

the maximum velocity by another 3× to 4× so that maximum target velocities in excess of 300 kph are trackable, making the IWR1642 sensor a suitable sensor for fast-moving traffic scenes such as those around highways and on-ramps

That is the reason we chose that sensor for our application:
Please clear the below questions:

Is that possible to achieve detection of 300km/h velocity with this sensor using IWR1642BOOT EVM, by just tuning configs and code?

Thanks in advance