This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
With the help of documentation and various threads out here I was able to run the sample use cases with out any hassle.
The problem that I have now is that running the matlab script "create_calib_coeffs.m" under "cascade_radar_object_detect" folder inside the
"..PROCESSOR_SDK_RADAR_03_08_00_00\vision_sdk\apps\src\rtos\radar\src\usecases\cascade_radar_object_detect" path, I see the following error,
"Unable to read file 'CC'. No such file or directory."
This looks like a missing file error to me, but what file do I need to place inside this directory make the script generate the coefficients as intended?
Thanks,
Saketh.