This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: Exposed Pad/Stencil dimensions missing from the datasheet - PN:TMP117NAIDRVR

Part Number: TMP117

Hello,

Datasheet Link: TMP117 High-Accuracy, Low-Power, Digital Temperature Sensor With SMBusTm- and I2C-Compatible Interface datasheet (Rev. C)

From the land-pattern section of package DRV0006B, exposed pad (1.6X1.0 is missing. Also stencil area of exposed pad is missing from the datasheet. I was asked by the the customer support to post my question on E2E forum as they did not find the correct answer to it. 

You may also confirm if the package DRV0006B is same as DRV0006A. 

Datasheet link for DRV0006Ahttps://www.ti.com/lit/gpn/TPS25200